This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请问CC2530的一些参考设计中,DEBUG接口中的SPI信号是干什么用的?
为了与TI的RF Studio通信,可以更好地配置、运行CC2530
CC2530是soc.用CCDEBUGER调试时,只需要DC DD Reset POWER Gnd 5跟线就够了。SPI口主要是考虑到如果你使用的是非SOC的RF IC,如CC1101 CC2520等,CCDEBUGER可以兼容。你可以看到,SOC类型的debug口上SPI是没有实际连接的。
谢谢你的回复。
但是在TI ZNP参考原理图中(swrr076.zip文件中的CC2530_ZNP_Schematic.pdf),用的是CC2530 SOC芯片,其DUBUG口也接着SPI,这和你说的不符。
你的观察很仔细。但是调试下载程序及配合PC软件,不需要SPI口(针对CC2530)。你可以把SPI相应的针口掰弯,不连接,一样可以。CC2530ZNP与cc2530还是有区别的。CC2530ZNP是网络处理器,需要外部增加MCU通过SPI或串口发送命令来控制zigbee的工作。
另外,CCDEBUGER的主芯片是CC2511,不排除未来修改固件,增加SPI的控制功能。