This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请教TI工程师AFE77xx系列芯片可以用于5G终端设计吗?

Other Parts Discussed in Thread: AFE7799

请教TI工程师:AFE77xx系列芯片可以用于5G终端设计吗?

AFE77xx芯片的载波频率切换和带宽切换时间是什么数量级?

  • 您可以在官网介绍页面获取详细信息

    www.ti.com.cn/.../AFE7799

    AFE7799 是一款高性能的多通道收发器,集成了四条直接上变频发送器链、四条直接下变频接收器链和两条宽带射频采样数字化辅助链(反馈路径)。发送器链和接收器链的高动态范围允许为无线基站生成和接收 2G、3G、4G 和 5G 信号。低功率耗散和大规模通道集成使得 AFE7799 适合在功率和尺寸两方面都受限的 4G 和 5G 大规模 MIMO 基站。

    关于载波频率切换和带宽切换时间,目前数据手册我没有看到确切数据,我会在核实后给您回复。
  • 以下是我在咨询相关专家后得到的回复

    The AFE77xx is intended for Base station, repeater, DAS, and active antenna systems. Though functional for terminal design, the device may be deemed overkill for that application.

    The carrier frequency is generated by internal PLL/VCO. Frequency change is completed through SPI programming. Taking into account the SPI programming speed and analog frequency calibration, the switching is not considered fast. However, there are multiple LOs so that for fast switching applications between two states, each LO can be programmed and then switched into place quickly. Further, there is an IF NCO that can change digitally quickly if carrier adjustment is needed within baseband bandwidth capabilities.