This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于CC1310 FEC的问题

Other Parts Discussed in Thread: CC1310, CC2500, CC1101

TI 工程师:

这里有两个问题:

1. 关于CC1310 的FEC , 我在以下两个地方看到有不一样的回答。

https://e2echina.ti.com/question_answer/wireless_connectivity/hw_rf_proprietary/f/45/t/180946?keyMatch=CC1310%20FEC&tisearch=Search-CN-everything :“FEC默认是开启的”

https://e2echina.ti.com/question_answer/wireless_connectivity/hw_rf_proprietary/f/45/p/163160/477626?keyMatch=CC1310%20FEC&tisearch=Search-CN-everything : “CC1310没有FEC,不过可以用软件自己做”

2. CC1310有FEC吗?

如果有,在哪里开启的呢? 与CC2500的FEC 相同吗?

如果没有,CC1310怎样与CC1101兼容通信呢?

谢谢!

  • 1. What's the modulation scheme of HSM?

    2. Does HSM adopt channel coding? If so, then what scheme is used?

    • 4mbps on CC1310 is coded using FEC and Viterbi decoder. The effective data rate is 4.0mbps the over-the-air is higher.
    • 1.5mbps on CC1310 is un-coded
    • 1.0mbps on CC1310 is un-coded
    • 5.0mbps on CC2650 is is coded using FEC and Viterbi decoder. The effective data rate is 4.0mbps the over-the-air is higher.
    • 2.0mbps on CC2650 is un-coded
    • 1.0mbps on CC2650 is un-coded

    3. How much overhead(includig syncword and preamble) is included in the HSM?

    • 32 bits of preamble and 32 bits of sync word is required and this is transmitted in 2FSK mode only, so therefore it effectively becomes more bits in 4 and 8FSK.

    4. Regarding the receiver sensitity, I have confirmed that the sensitivity level is -84dBm in this forum.

    • Yes, that is correct.

    But I couldn't see the BER which resulted in -84dBm. I want to know the specification on the receiver sensitivity of HSM.

    • 1% BER

    5. Does TI support the HSM in RF studio? If so, I want to know the approximate schedule of the software release.

    • Not yet, but it will be included in an upcoming version. However the Patches required for TIRTOS to work at these data rates is included in the latest TI-RTOS bundle and the PER example code shows how to use it.

    6. I heard that the 1.6Mbps example using 4FSK scheme is possilbe in this forum.

    • Yes, that is correct, but we have de-tuned it to run at 1.5mbps maximum. This is not released yet.
  • 4 mbps PHY已经实现FEC,因此您不能通过任何方式打开/关闭或配置它。
  • 请问下CC1310 “5 kbps, Simple Link Long Range (Mode 2). 20 ksps, DSSS = 2” LRM, 有实现FEC吗? FEC 配置与CC2500相同(之前有使用CC2500FEC)?谢谢
  • 有没有关于CC1310 FEC 相关的介绍呢?有看到一篇Design Note DN50,但没有看到有包含CC1310。谢谢
  • 这方面确实不太多,您可以看一下下面的链接

    这个是与CC1101上使用的FEC兼容的FEC补丁

    dev.ti.com/.../cc1101-migration.html