Other Parts Discussed in Thread: CC1310
用CC1310做了一个板子,由于板子比较小,就用两个颗氧化银纽扣电池(一颗电量为8.3mAh,两颗电池串联)供电,设置为433MHz,GFSK,50Kbps,射频功率设置在10dBm,程序设置为上电后休眠,休眠之后再开射频发送数据(easylinkTX异步发送),经过测量,发送前10ms会将电池电压拉下1.2v左右,之后单片机就开始工作不正常,射频一直在发送,发送的都是乱码。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: CC1310
用CC1310做了一个板子,由于板子比较小,就用两个颗氧化银纽扣电池(一颗电量为8.3mAh,两颗电池串联)供电,设置为433MHz,GFSK,50Kbps,射频功率设置在10dBm,程序设置为上电后休眠,休眠之后再开射频发送数据(easylinkTX异步发送),经过测量,发送前10ms会将电池电压拉下1.2v左右,之后单片机就开始工作不正常,射频一直在发送,发送的都是乱码。
电池3V的吗?两颗串联超电压了吧。可以把两颗并联减小内阻。
你可以参考一下文档:swra349 Coin cells and peak current draw.pdf
Optimizing for coin cell operation @ +10dBM: http://www.ti.com/lit/an/swra636b/swra636b.pdf
BR, Albin
灰小子 说:估计是电池放电电流比较小,建议换个放电电流大点的电池。可以先给电池并联一个电容做测试看看
那个文档就是给你一些解决问题的思路的
你可以用示波器看一下电压,如果都是brownout reset, 你确实需要更改供电方式,或者降低输出功率减低电流的
当你包大于一定长度的时候,你需要增加pump电容的。这个值你需要计算的.
BR. AZ