This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于应用 CC1350 LAUNCHPAD 在CCS 10 下烧录CC1310模块的问题

Other Parts Discussed in Thread: CC1310, CC1350

各位专家:现在我想通过CC1350 LAUNCHPAD 在CCS 10 环境下烧录CC1310模块不成功,有以下问题请教:

1、我已经将我的 CC1310 模块debug 接口连接到CC1350 LAUNCHPAD 相应调试接口,通过 flash programer 2 识别出我的CC1310 模块并成功烧录了 .out 文件。

2、现在我想通过 在 CCS 10 环境下 LOAD .OUT 文件,提示相应错误,请大家帮忙分析。

3、我通过修改 Target Configuration 并修改设备 为 CC1310F128, TCLK FREQUENCY 为2.5M 。   进行 CONNECT TEST提示出现如下问题。

[Start: Texas Instruments XDS110 USB Debug Probe_0]

Execute the command:

%ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -rv -o -S integrity

[Result]


-----[Print the board config pathname(s)]------------------------------------

C:\Users\ADMINI~1\AppData\Local\TEXASI~1\
CCS\ccs1000\0\0\BrdDat\testBoard.dat

-----[Print the reset-command software log-file]-----------------------------

This utility has selected a 100- or 510-class product.
This utility will load the adapter 'jioxds110.dll'.
The library build date was 'Feb 13 2020'.
The library build time was '18:30:11'.
The library package version is '9.1.0.00001'.
The library component version is '35.35.0.0'.
The controller does not use a programmable FPGA.
The controller has a version number of '5' (0x00000005).
The controller has an insertion length of '0' (0x00000000).
This utility will attempt to reset the controller.
This utility has successfully reset the controller.

-----[Print the reset-command hardware log-file]-----------------------------

The scan-path will be reset by toggling the JTAG TRST signal.
The controller is the XDS110 with USB interface.
The link from controller to target is direct (without cable).
The software is configured for XDS110 features.
The controller cannot monitor the value on the EMU[0] pin.
The controller cannot monitor the value on the EMU[1] pin.
The controller cannot control the timing on output pins.
The controller cannot control the timing on input pins.
The scan-path link-delay has been set to exactly '0' (0x0000).

An error occurred while hard opening the controller.

-----[An error has occurred and this utility has aborted]--------------------

This error is generated by TI's USCIF driver or utilities.

The value is '-242' (0xffffff0e).
The title is 'SC_ERR_ROUTER_ACCESS_SUBPATH'.

The explanation is:
A router subpath could not be accessed.
The board configuration file is probably incorrect.

[End: Texas Instruments XDS110 USB Debug Probe_0]

请教上述问题如何处理,什么原因造成的。

是否不能通过CC1350 开发板通过 CCS 10 对CC1310 模块下载程序。

CCCC1350 开发板上开发的例程是针对 CC1350 模块的,是否需经过修改才可下载到CC1310模块。

以上问题请教大家。