我根据adcbufcontinuous的提示更改代码想要四信道adc采集但是只能读出单通道数据
* ======== adcBufContinuousSampling.c ========
*/
#include <stdint.h>
#include <stdio.h>
/* For sleep() */
#include <unistd.h>
*/
#include <stdint.h>
#include <stdio.h>
/* For sleep() */
#include <unistd.h>
/* Driver Header files */
#include <ti/drivers/ADCBuf.h>
#include <ti/drivers/UART.h>
#include <ti/drivers/ADCBuf.h>
#include <ti/drivers/UART.h>
/* Example/Board Header files */
#include "Board.h"
#include "Board.h"
#define ADCBUFFERSIZE (64)
#define UARTBUFFERSIZE ((20* ADCBUFFERSIZE) + 24)
#define UARTBUFFERSIZE ((20* ADCBUFFERSIZE) + 24)
uint16_t sampleBufferOne[ADCBUFFERSIZE/4];
uint16_t sampleBufferTwo[ADCBUFFERSIZE/4];
uint16_t sampleBufferOne2[ADCBUFFERSIZE/4];
uint16_t sampleBufferTwo2[ADCBUFFERSIZE/4];
uint16_t sampleBufferOne3[ADCBUFFERSIZE/4];
uint16_t sampleBufferTwo3[ADCBUFFERSIZE/4];
uint16_t sampleBufferOne4[ADCBUFFERSIZE/4];
uint16_t sampleBufferTwo4[ADCBUFFERSIZE/4];
uint32_t microVoltBuffer[ADCBUFFERSIZE];
uint32_t buffersCompletedCounter = 0;
char uartTxBuffer[UARTBUFFERSIZE];
uint16_t sampleBufferTwo[ADCBUFFERSIZE/4];
uint16_t sampleBufferOne2[ADCBUFFERSIZE/4];
uint16_t sampleBufferTwo2[ADCBUFFERSIZE/4];
uint16_t sampleBufferOne3[ADCBUFFERSIZE/4];
uint16_t sampleBufferTwo3[ADCBUFFERSIZE/4];
uint16_t sampleBufferOne4[ADCBUFFERSIZE/4];
uint16_t sampleBufferTwo4[ADCBUFFERSIZE/4];
uint32_t microVoltBuffer[ADCBUFFERSIZE];
uint32_t buffersCompletedCounter = 0;
char uartTxBuffer[UARTBUFFERSIZE];
/* Driver handle shared between the task and the callback function */
UART_Handle uart;
UART_Handle uart;
/*
* This function is called whenever an ADC buffer is full.
* The content of the buffer is then converted into human-readable format and
* sent to the PC via UART.
*/
void adcBufCallback(ADCBuf_Handle handle, ADCBuf_Conversion *conversion,
void *completedADCBuffer, uint32_t completedChannel)
{
uint_fast16_t i;
uint_fast16_t uartTxBufferOffset = 0;
* This function is called whenever an ADC buffer is full.
* The content of the buffer is then converted into human-readable format and
* sent to the PC via UART.
*/
void adcBufCallback(ADCBuf_Handle handle, ADCBuf_Conversion *conversion,
void *completedADCBuffer, uint32_t completedChannel)
{
uint_fast16_t i;
uint_fast16_t uartTxBufferOffset = 0;
/* Adjust raw ADC values and convert them to microvolts */
ADCBuf_adjustRawValues(handle, completedADCBuffer, ADCBUFFERSIZE,
completedChannel);
ADCBuf_convertAdjustedToMicroVolts(handle, completedChannel,
completedADCBuffer, microVoltBuffer, ADCBUFFERSIZE);
ADCBuf_adjustRawValues(handle, completedADCBuffer, ADCBUFFERSIZE,
completedChannel);
ADCBuf_convertAdjustedToMicroVolts(handle, completedChannel,
completedADCBuffer, microVoltBuffer, ADCBUFFERSIZE);
/* Start with a header message. */
uartTxBufferOffset = snprintf(uartTxBuffer,
UARTBUFFERSIZE - uartTxBufferOffset, "\r\nBuffer %u finished.",
(unsigned int)buffersCompletedCounter++);
uartTxBufferOffset = snprintf(uartTxBuffer,
UARTBUFFERSIZE - uartTxBufferOffset, "\r\nBuffer %u finished.",
(unsigned int)buffersCompletedCounter++);
/* Write raw adjusted values to the UART buffer if there is room. */
uartTxBufferOffset += snprintf(uartTxBuffer + uartTxBufferOffset,
UARTBUFFERSIZE - uartTxBufferOffset, "\r\nRaw Buffer: ");
uartTxBufferOffset += snprintf(uartTxBuffer + uartTxBufferOffset,
UARTBUFFERSIZE - uartTxBufferOffset, "\r\nRaw Buffer: ");
for (i = 0; i < ADCBUFFERSIZE && uartTxBufferOffset < UARTBUFFERSIZE; i++) {
uartTxBufferOffset += snprintf(uartTxBuffer + uartTxBufferOffset,
UARTBUFFERSIZE - uartTxBufferOffset, "%u,",
*(((uint16_t *)completedADCBuffer) + i));
}
uartTxBufferOffset += snprintf(uartTxBuffer + uartTxBufferOffset,
UARTBUFFERSIZE - uartTxBufferOffset, "%u,",
*(((uint16_t *)completedADCBuffer) + i));
}
/* Write microvolt values to the UART buffer if there is room. */
if (uartTxBufferOffset < UARTBUFFERSIZE) {
uartTxBufferOffset += snprintf(uartTxBuffer + uartTxBufferOffset,
UARTBUFFERSIZE - uartTxBufferOffset, "\r\nMicrovolts: ");
if (uartTxBufferOffset < UARTBUFFERSIZE) {
uartTxBufferOffset += snprintf(uartTxBuffer + uartTxBufferOffset,
UARTBUFFERSIZE - uartTxBufferOffset, "\r\nMicrovolts: ");
for (i = 0; i < ADCBUFFERSIZE && uartTxBufferOffset < UARTBUFFERSIZE; i++) {
uartTxBufferOffset += snprintf(uartTxBuffer + uartTxBufferOffset,
UARTBUFFERSIZE - uartTxBufferOffset, "%u,",
(unsigned int)microVoltBuffer[i]);
}
}
uartTxBufferOffset += snprintf(uartTxBuffer + uartTxBufferOffset,
UARTBUFFERSIZE - uartTxBufferOffset, "%u,",
(unsigned int)microVoltBuffer[i]);
}
}
/*
* Ensure we don't write outside the buffer.
* Append a newline after the data.
*/
if (uartTxBufferOffset < UARTBUFFERSIZE) {
uartTxBuffer[uartTxBufferOffset++] = '\n';
}
else {
uartTxBuffer[UARTBUFFERSIZE-1] = '\n';
}
* Ensure we don't write outside the buffer.
* Append a newline after the data.
*/
if (uartTxBufferOffset < UARTBUFFERSIZE) {
uartTxBuffer[uartTxBufferOffset++] = '\n';
}
else {
uartTxBuffer[UARTBUFFERSIZE-1] = '\n';
}
/* Display the data via UART */
UART_write(uart, uartTxBuffer, uartTxBufferOffset);
}
UART_write(uart, uartTxBuffer, uartTxBufferOffset);
}
/*
* Callback function to use the UART in callback mode. It does nothing.
*/
void uartCallback(UART_Handle handle, void *buf, size_t count) {
return;
}
* Callback function to use the UART in callback mode. It does nothing.
*/
void uartCallback(UART_Handle handle, void *buf, size_t count) {
return;
}
/*
* ======== mainThread ========
*/
void *mainThread(void *arg0)
{
UART_Params uartParams;
ADCBuf_Handle adcBuf;
ADCBuf_Params adcBufParams;
ADCBuf_Conversion continuousConversion[4];
* ======== mainThread ========
*/
void *mainThread(void *arg0)
{
UART_Params uartParams;
ADCBuf_Handle adcBuf;
ADCBuf_Params adcBufParams;
ADCBuf_Conversion continuousConversion[4];
/* Call driver init functions */
ADCBuf_init();
UART_init();
ADCBuf_init();
UART_init();
/* Create a UART with data processing off. */
UART_Params_init(&uartParams);
uartParams.writeDataMode = UART_DATA_BINARY;
uartParams.writeMode = UART_MODE_CALLBACK;
uartParams.writeCallback = uartCallback;
uartParams.baudRate = 115200;
uart = UART_open(Board_UART0, &uartParams);
UART_Params_init(&uartParams);
uartParams.writeDataMode = UART_DATA_BINARY;
uartParams.writeMode = UART_MODE_CALLBACK;
uartParams.writeCallback = uartCallback;
uartParams.baudRate = 115200;
uart = UART_open(Board_UART0, &uartParams);
/* Set up an ADCBuf peripheral in ADCBuf_RECURRENCE_MODE_CONTINUOUS */
ADCBuf_Params_init(&adcBufParams);
adcBufParams.callbackFxn = adcBufCallback;
adcBufParams.recurrenceMode = ADCBuf_RECURRENCE_MODE_CONTINUOUS;
adcBufParams.returnMode = ADCBuf_RETURN_MODE_CALLBACK;
adcBufParams.samplingFrequency = 200;
adcBuf = ADCBuf_open(Board_ADCBUF0, &adcBufParams);
ADCBuf_Params_init(&adcBufParams);
adcBufParams.callbackFxn = adcBufCallback;
adcBufParams.recurrenceMode = ADCBuf_RECURRENCE_MODE_CONTINUOUS;
adcBufParams.returnMode = ADCBuf_RETURN_MODE_CALLBACK;
adcBufParams.samplingFrequency = 200;
adcBuf = ADCBuf_open(Board_ADCBUF0, &adcBufParams);
/* Configure the conversion struct */
continuousConversion[0].arg = NULL;
continuousConversion[0].adcChannel = 2;
continuousConversion[0].sampleBuffer = sampleBufferOne;
continuousConversion[0].sampleBufferTwo = sampleBufferTwo;
continuousConversion[0].samplesRequestedCount = ADCBUFFERSIZE/4;
continuousConversion[0].arg = NULL;
continuousConversion[0].adcChannel = 2;
continuousConversion[0].sampleBuffer = sampleBufferOne;
continuousConversion[0].sampleBufferTwo = sampleBufferTwo;
continuousConversion[0].samplesRequestedCount = ADCBUFFERSIZE/4;
continuousConversion[1].arg = NULL;
continuousConversion[1].adcChannel = 3;
continuousConversion[1].sampleBuffer = sampleBufferOne2;
continuousConversion[1].sampleBufferTwo = sampleBufferTwo2;
continuousConversion[1].samplesRequestedCount = ADCBUFFERSIZE/4;
continuousConversion[1].adcChannel = 3;
continuousConversion[1].sampleBuffer = sampleBufferOne2;
continuousConversion[1].sampleBufferTwo = sampleBufferTwo2;
continuousConversion[1].samplesRequestedCount = ADCBUFFERSIZE/4;
continuousConversion[2].arg = NULL;
continuousConversion[2].adcChannel = 4;
continuousConversion[2].sampleBuffer = sampleBufferOne3;
continuousConversion[2].sampleBufferTwo = sampleBufferTwo3;
continuousConversion[2].samplesRequestedCount = ADCBUFFERSIZE/4;
continuousConversion[3].arg = NULL;
continuousConversion[3].adcChannel = 5;
continuousConversion[3].sampleBuffer = sampleBufferOne4;
continuousConversion[3].sampleBufferTwo = sampleBufferTwo4;
continuousConversion[3].samplesRequestedCount = ADCBUFFERSIZE/4;
if (adcBuf == NULL){
/* ADCBuf failed to open. */
while(1);
}
/* Start converting. */
if (ADCBuf_convert(adcBuf, continuousConversion, 4) !=
ADCBuf_STATUS_SUCCESS) {
/* Did not start conversion process correctly. */
while(1);
}
if (ADCBuf_convert(adcBuf, continuousConversion, 4) !=
ADCBuf_STATUS_SUCCESS) {
/* Did not start conversion process correctly. */
while(1);
}
/*
* Go to sleep in the foreground thread forever. The ADC hardware will
* perform conversions and invoke the callback function when a buffer is
* full.
*/
while(1) {
sleep(1000);
}
}
* Go to sleep in the foreground thread forever. The ADC hardware will
* perform conversions and invoke the callback function when a buffer is
* full.
*/
while(1) {
sleep(1000);
}
}
如果将
if (ADCBuf_convert(adcBuf, continuousConversion, 4) !=
ADCBuf_STATUS_SUCCESS) {
/* Did not start conversion process correctly. */
while(1);
}
中的continuousConversion[4]改为 continuousConversion[0]、 continuousConversion[1]、 continuousConversion[2]、 continuousConversion[3]
均只能读出单个通道的数据
这是为什么
应该如何更改