This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC85XXDK EHIF疑问

Other Parts Discussed in Thread: MSP430F5438, CC8531, CC2530

我有两个CC85XXDK板,想主从设备都工作于Host control模式。

在PurePath Wireless Configurator中,已经配置主设备为"Stereo output base station"、"Host control",从设备配置为"Stereo input satellite"、"Host control"。

然后在PurePath Wireless Commander中,通过EHIF指令,已经成功完成两个设备的配对。

但是,我在从设备连接音频源,在主设备为啥没声音出来呢?

  • 其中,主设备端的Audio Streaming设置如下:

  • 图片贴不了,我文字说明一下吧。

    主设备端的Audio Streaming设置为:

    logical channel:Input left, Input right。

    从设备在通过NWM_ACH_SET_USAGE指令来设置Audio channel。

  • 用commander发EHIF指令,interesting. 如下是EHIF接口的源代码及操作步骤。你可以借鉴代码中的步骤来做一下。

    http://e2e.ti.com/support/low_power_rf/f/382/t/115370.aspx

    Step-by-step:

    1. Download and extract the zip.

    2. Open the PurePath Wireless Configurator (downloadable from here: www.ti.com/ppwc), and open the project CC85XXDK Preloaded Demo (available from Start Page).

    3. Flash one CC85xx device with the master device configuraton as is.

    4. Flash one CC85xx device with the slave device configuraton with the following modifications: - Select host-controlled operation. - In the IO mapping panel set the "External host interface interrupt" pin to GIO3.

    5. Connect the MSP430F5438 Experimenter Board to the slave Audio EB like shown in EHIF_Connection_MSP430.pdf (included in the zip).

    6. Program the MSP430F5438 either by debugging in IAR or flash it using the SmartRF Flash Programmer. Feel free to ask if anything is unclear. Enjoy!

  • 问题已经解决了,哈哈。主设备端要设置音量才行,不然默认是没有声音播出的。

    另外,我现在已经成功使用CC2530和CC8531通信,主从设备都工作于Host control模式。

    我有个问题再想请教,CC2530和CC8531都工作于2.4G,同时使用会有频段干扰的问题吗?

  • CC8531和cc2530频道确实有重叠。不过,CC8531采用跳频工作的方式,CC2530是频道扫描确定一个信道后会固定在这个信道工作。

    cc2530传少量数据。CC8531数据量较大。另外,你可以看CC2530和CC8531的blocking和selectivty参数,业界来说还是很优秀的。

  • 你好。我遇到了跟你同样的问题。请问你音量只设置了 master那一端吗。VC_SET_VOLUME 命令的参数是什么呢。

    我的硬件是自己贴的两块CC85XXDK-HEADSET 板子。在Autonomous模式下工作是正常的。

    purepath wireless configurator 里面我选的是CC85XX preloaded demo 。但我master做的是音频输入。slave是做的音频输出