Other Parts Discussed in Thread: CC1310
看到数据手册上面写着,SCE每秒进行一次12位的ADC采样,采样电流位0.95uA,我运行了TI SDK中的rfWsnNode例程。该例程的说明是每秒进行一次ADC采样,变化的值大于设置的掩码即唤醒MCU进行发送,我更改了触发事件的内容,即ADC采样的电压值大于3V即唤醒单片机进行无线发送,功能已经实现,并且把程序中display相关操作全部停止,用专门测量电流的仪器进行测量,在只有采样的时候电流位3.5mA,发送接收时候9--10mA,有时会跳到20多mA.请问,1,这个例程中,在ADC进行采样的时候主MCU是处在睡眠状态,然后由ADC事件来唤醒的么? 2,我测量过rfEASYLinkTX例程 ,一直处在发送状态下的功耗位6--7mA,那rfWsnNode例程电流跳到20mA是处在什么状态呢? 9-10mA的状态应该是发送的同时还有在继续ADC采样,怎么停止ADC任务呢? 3,如何才能达到那样的超低功耗ADC采样来唤醒单片机? 4.找了好多资料 ,但是一直没有找到关于CC1310各种功能函数的API接口 ,请问能发个网址或者资料给我么 ?万分感谢!!