Other Parts Discussed in Thread: CC1310
CC1310 NORTOS的 有定时器使用demo例程吗
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
GPTimerCC26XX_Params params;
params.width = GPT_CONFIG_32BIT;
params.mode = GPT_MODE_ONESHOT_UP;
params.debugStallMode = GPTimerCC26XX_DEBUG_STALL_OFF;
hTimer = GPTimerCC26XX_open(Board_GPTIMER0A, ¶ms);
if(hTimer == NULL)
{
while(1);
}
rxTimeoutVal = (SysCtrlClockGet()*3UL)/10UL - 1UL;
GPTimerCC26XX_setLoadValue(hTimer, rxTimeoutVal);
GPTimerCC26XX_registerInterrupt(hTimer, rxTimeoutCb, GPT_INT_TIMEOUT);
GPTimerCC26XX_start(hTimer);
void rxTimeoutCb(GPTimerCC26XX_Handle handle,
GPTimerCC26XX_IntMask interruptMask)
{
GPTimerCC26XX_setLoadValue(hTimer, rxTimeoutVal);
PIN_setOutputValue(pinHandle, Board_PIN_LED2,!PIN_getOutputValue(Board_PIN_LED2));
//GPTimerCC26XX_start(hTimer);
}
请问要怎么样设置才能使定时器重复进入中断?
必须要在回调函数里面每次去 start吗?
你要用GPTimer的什么模式?下面是我配置的下降沿中断检测的代码,每次检测到下降沿,就打印感叹号:
/***** Includes *****/
/* Standard C Libraries */
#include <stdlib.h>
#include <stdio.h>
/* RTOS header files */
#include <ti/sysbios/BIOS.h>
#include <ti/sysbios/knl/Task.h>
/* TI Drivers */
#include <ti/drivers/rf/RF.h>
#include <ti/drivers/PIN.h>
#include <ti/drivers/pin/PINCC26XX.h>
#include <ti/drivers/timer/GPTimerCC26XX.h>
/* Driverlib Header files */
#include DeviceFamily_constructPath(driverlib/rf_prop_mailbox.h)
/* Board Header files */
#include "Board.h"
/***** Variable declarations *****/
/* Pin driver handle */
static PIN_Handle ledPinHandle;
static PIN_State ledPinState;
PIN_Config pinTable[] =
{
IOID_0 | PIN_INPUT_EN | PIN_PULLUP | PIN_IRQ_NEGEDGE ,
PIN_TERMINATE
};
GPTimerCC26XX_Handle hTimer0A;
//static uint8_t counter = 0;
void timerCallback0A(GPTimerCC26XX_Handle handle, GPTimerCC26XX_IntMask interruptMask)
{
printf("!\n");
}
/***** Function definitions *****/
void *mainThread(void *arg0)
{
/* Open LED pins */
ledPinHandle = PIN_open(&ledPinState, pinTable);
if (ledPinHandle == NULL)
{
while(1);
}
GPTimerCC26XX_Params params0A;
GPTimerCC26XX_Params_init(¶ms0A);
params0A.width = GPT_CONFIG_16BIT;
params0A.mode = GPT_MODE_EDGE_COUNT_UP;
params0A.debugStallMode = GPTimerCC26XX_DEBUG_STALL_OFF;
hTimer0A = GPTimerCC26XX_open(CC2640R2_LAUNCHXL_GPTIMER0A, ¶ms0A);
if(hTimer0A == NULL)
{
while(1);
}
GPTimerCC26XX_registerInterrupt(hTimer0A, timerCallback0A, GPT_INT_CAPTURE_MATCH);
GPTimerCC26XX_PinMux pinMux = GPTimerCC26XX_getPinMux(hTimer0A);
PINCC26XX_setMux(ledPinHandle, IOID_0, pinMux);
GPTimerCC26XX_setCaptureEdge(hTimer0A, GPTimerCC26XX_NEG_EDGE);
GPTimerCC26XX_setLoadValue(hTimer0A, 0xFFFFFF);
GPTimerCC26XX_setMatchValue(hTimer0A, 1);
GPTimerCC26XX_start(hTimer0A);
while(1)
{
Task_sleep(BIOS_WAIT_FOREVER);
}
}