This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1101空中唤醒模式Tevent0时间段内平均电流怎么计算?



halSpiWriteReg(CCxxx0_WOREVT1, 0x6f); 
halSpiWriteReg(CCxxx0_WOREVT0, 0xcE); //
halSpiWriteReg(CCxxx0_WORCTRL, 0x48); //
halSpiWriteReg(CCxxx0_MCSM2, 0x01); //

halSpiWriteReg(CCxxx0_MCSM0, 0x18); //以上是代码中对WOR模式的设置部分,然后根据swra126b手册计算t event1=16*750/26000000=0.462ms,

Tsleep =750*384/26000000=11.08ms,根据公式3 算出Tevent0 min大概13.32ms,EVENT0=0X6FCE=28622,算出Tevent0=825.6ms>13.32ms,那么请问一下,在Tevent1的时间内接受电流大概16mA,整段Tevent0的时间段内的平均电流是16*0.462/825.6这样计算吗?

以上是我根据手册自己推算的,不知道有没有问题,麻烦帮忙看看怎么计算这个平均电流?