Other Parts Discussed in Thread: CC1312R, CC1310
工程师你好!
看到SmartRF Studio里433MHz可以配置到1500kbps,直连情况下还是可以通讯的,用天线则效果很差,不确定是否为外围电路为868MHz的原因。
想请教一下CC1312R 在433MHz下的最快速率到1500kbps吗?
如果2GFSK不行,像CC1310一样使用4FSK模式可以达到最快速率是多少?
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
工程师你好!
看到SmartRF Studio里433MHz可以配置到1500kbps,直连情况下还是可以通讯的,用天线则效果很差,不确定是否为外围电路为868MHz的原因。
想请教一下CC1312R 在433MHz下的最快速率到1500kbps吗?
如果2GFSK不行,像CC1310一样使用4FSK模式可以达到最快速率是多少?
谢谢!
看到SmartRF Studio里433MHz可以配置到1500kbps,直连情况下还是可以通讯的,用天线则效果很差
直连是通过什么方式连接的,设置为1500kbps从哪里设置的,传一下截图
CC1310的4FSK模式仅用来测试,CC1312R上没有这个测试