以MSP430F5438+CC2564的LSR芯片做的蓝牙设备,跑Stonestreet One里面的SPP Demo,在启动栈的时候总会报-4的错误,代码没改。硬件连接按照代码的要求做的,求解释!
P.S. Stonestreet One里面MSP430F5438是不是用Uart1与PC通信,Uart2与CC2564通信?在直接跑Demo的时候对于代码有需要的改动么?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
以MSP430F5438+CC2564的LSR芯片做的蓝牙设备,跑Stonestreet One里面的SPP Demo,在启动栈的时候总会报-4的错误,代码没改。硬件连接按照代码的要求做的,求解释!
P.S. Stonestreet One里面MSP430F5438是不是用Uart1与PC通信,Uart2与CC2564通信?在直接跑Demo的时候对于代码有需要的改动么?
Hi Haixiang,
5438的板子上需要一个RF3 connector, 其实就是需要一些线的连接, 请看如下:
http://processors.wiki.ti.com/index.php/CC256X_MSP:EXP430F5438#RF3_Connector
Haixiang您好。
SPP demo在运行的时候,代码无需修改。您的协议栈初始化报错有可能是因为MSP430F5438和CC2564之间的串口没有通。
确实是MSP430F5438用USCI_A1来和PC通信,用USCI_A2来和CC2564通信。
不知道您是用的MSP430F5438的评估板做的测试,还是在您自己画的板子上作测试。
如果您是在MSP430F5438的评估板,在USCI_A2处是需要飞线的,不知道您有否注意到。
如果是您自己画的板子,最好能够测量一下USCI_A2上是否有串口信号。自己的板子上时钟的质量如何。
任何问题您可以和我联系,nina.li@wi-linktech.com