This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1310: 使用SysCtrlSystemReset复位芯片卡死

Part Number: CC1310


使用SysCtrlSystemReset对程序进行复位,经常性卡死,

1. 供电:4.2V锂电池->3.3VLDO->1310

2. 5V电压经USB通过另一块PMIC芯片对电池进行充电,IO引脚检测充电器拔出,进行系统复位,大概率性系统死机

3.程序起始位置点亮LED, 复位前熄灭LED,死机后LED未点亮

4.程序在15.4协议栈版本,仅RTOS版本,和无RTOS版本均测试出相同问题,大概率卡死