上电启动后CPU GPIO和脉冲计数器功能可以正常工作;但是无线发送一条后GPIO功能不能驱动引脚,脉冲计数器(定时器)不能正常那个工作;
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
但是无线发送一条后GPIO功能不能驱动引脚,脉冲计数器(定时器)不能正常那个工作;
正常情况下无线发送不会影响其他部分,检查下是否存在引脚复用
程序中只有一个线程,在启动后会过10秒后才会进行无线数据发送,发送之前数据采集是没有问题的,只要进行无线数据发送,引脚驱动和计数器就不能工作了,如果是引脚复用初始化之后程序运行之前应该就不能工作了,现在是刚开始可以。目前没有尝试其他功能,只用到了一个引脚写了一个传感器的驱动,还有一个计数器功能,这两个都会受到影响
两个计数器,计数之后发送出去,引脚驱动也是类似代码,指示计数器部分变成了引脚驱动读取传感器数据;代码如下
void timerCallback_50ms(GPTimerCC26XX_Handle handle, GPTimerCC26XX_IntMask interruptMask)
{
PIN_setOutputValue(POWT1PinHandle, CC1310_LAUNCHXL_PIN_POWT1, 0);
PIN_setOutputValue(POWT2PinHandle, CC1310_LAUNCHXL_PIN_POWT2, 0);
//GPTimerCC26XX_disableInterrupt(hTimer_50ms,GPT_MODE_ONESHOT_UP);
GPTimerCC26XX_stop(hTimer_50ms);
DataValueInit_Value.Temp1=GPTimerCC26XX_getValue(hTimer_count_1);
DataValueInit_Value.Temp2=GPTimerCC26XX_getValue(hTimer_count_2);
GPTimerCC26XX_clearValue(hTimer_count_1,0);
GPTimerCC26XX_clearValue(hTimer_count_2,0);
GPTimerCC26XX_stop(hTimer_count_1);
GPTimerCC26XX_stop(hTimer_count_2);
DataValueInit_Value.Temp_Flag=1;
PIN_setConfig(T1PinHandle, PIN_BM_OUTPUT_MODE | PIN_BM_INPUT_MODE, CC1310_LAUNCHXL_PIN_T1 | PIN_GPIO_OUTPUT_EN | PIN_GPIO_LOW | PIN_PUSHPULL | PIN_INPUT_DIS|PIN_DRVSTR_MED);
PIN_setConfig(T2PinHandle, PIN_BM_OUTPUT_MODE | PIN_BM_INPUT_MODE, CC1310_LAUNCHXL_PIN_T2 | PIN_GPIO_OUTPUT_EN | PIN_GPIO_LOW | PIN_PUSHPULL | PIN_INPUT_DIS|PIN_DRVSTR_MED);
}
void Detect_Temperature(void)
{
PIN_setConfig(T1PinHandle, PIN_BM_OUTPUT_MODE | PIN_BM_INPUT_MODE, CC1310_LAUNCHXL_PIN_T1 | PIN_GPIO_OUTPUT_DIS | PIN_INPUT_EN | PIN_PULLUP);
PIN_setConfig(T2PinHandle, PIN_BM_OUTPUT_MODE | PIN_BM_INPUT_MODE, CC1310_LAUNCHXL_PIN_T2 | PIN_GPIO_OUTPUT_DIS | PIN_INPUT_EN | PIN_PULLUP);
PIN_setOutputValue(POWT1PinHandle, CC1310_LAUNCHXL_PIN_POWT1, 1);
PIN_setOutputValue(POWT2PinHandle, CC1310_LAUNCHXL_PIN_POWT2, 1);
GPTimerCC26XX_start(hTimer_50ms);
GPTimerCC26XX_enableInterrupt(hTimer_50ms,GPT_MODE_ONESHOT_UP);
GPTimerCC26XX_start(hTimer_count_1);
//CT1820B_Temp_Conv();
GPTimerCC26XX_start(hTimer_count_2);
}
void Result_Temperature(void)
{
DataValueInit_Value.Temp1_Value=Temp_Value(DataValueInit_Value.Temp1);
DataValueInit_Value.Temp2_Value=Temp_Value(DataValueInit_Value.Temp2);
}
void txFunctionUpdate(void)
{
uint16_t RealtimeVoltage=0;//,Temperature1=0,Temperature2=0;
uint16_t BatteryState=0;
/* Create packet with incrementing sequence number and random payload */
BatteryState=(0x0001&scifTaskData.dataStream.state.batteryState)<<1;
if((timeCount > 5)||abs(RealtimeVoltage - LastRealtimeVoltage) > DataValueInit_Value.BurstThreshold||Switchupdateflag==1)//定时和突变上传
{
timeCount=0;
/* Call txFunction initialization */
txFunctionInit();
lbtPacket.payload[0] = (uint8_t)(DataValueInit_Value.seqNumber);
lbtPacket.payload[1] = (uint8_t)(DataValueInit_Value.seqNumber>>8);
lbtPacket.payload[2] = (uint8_t)(DataValueInit_Value.seqNumber>>16);
lbtPacket.payload[3] = (uint8_t)(DataValueInit_Value.seqNumber>>24);
lbtPacket.payload[4] = (uint8_t)DataValueInit_Value.Temp1_Value;
lbtPacket.payload[5] = (uint8_t)(DataValueInit_Value.Temp1_Value>>8);
lbtPacket.payload[6] = (uint8_t)(SwitchState+BatteryState);
lbtPacket.payload[7] = (uint8_t)(sendframecounter);
lbtPacket.payload[8] = (uint8_t)(sendframecounter>>8);
sendframecounter++;
if(sendframecounter%10==0)
{
SendframeUpdate(&sendframecounter);
}
lbtPacket.len = RFEASYLINKLBT_PAYLOAD_LENGTH;
lbtPacket.dstAddr[0] = 0xF3;
lbtPacket.absTime = 0;
EasyLink_transmitCcaAsync(&lbtPacket, lbtDoneCb);
}
timeCount++;
}
while(1)
{
// Wait for an ALERT callback
// Semaphore_pend(Semaphore_handle(&semScTaskAlert), BIOS_WAIT_FOREVER);
if(KeyMsg)
{
KeyMsg=0;
Detect_Temperature();
sleep(1);
}
if(DataValueInit_Value.Temp_Flag==1)
{
Result_Temperature();
DataValueInit_Value.Temp_Flag=2;
KeyMsg=1;
}
Key_ProcessUpdate();
ADCInit();
PIN_setOutputValue(RunPinHandle, CC1310_LAUNCHXL_PIN_RUNLED, (PIN_getOutputValue(CC1310_LAUNCHXL_PIN_RUNLED))?0:1);
Send_Flag++;
if(Send_Flag==20)
{
Send_Flag=0;
if(DataValueInit_Value.Temp_Flag==2)
{
txFunctionUpdate();
}
}
}