This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI CC1310 15.4 simplelink_cc13x0_sdk_4_20_00_05 / sensor MAC 添加代码如下,其他未做任何更改
sensor 79 行 --85行 代码
#include "hw_memmap.h"
#include "hw_fcfg1.h"
#include "hw_types.h"
uint64_t macAddrLsb;
uint64_t macAddrMsb;
uint64_t macAddress;
427--429 行 代码
macAddrLsb = HWREG(FCFG1_BASE + FCFG1_O_MAC_15_4_0);
macAddrMsb = HWREG(FCFG1_BASE + FCFG1_O_MAC_15_4_1);
macAddress = (uint64_t)(macAddrMsb << 32) + macAddrLsb;
---》debug---》Expressions macAddrLsb / macAddrMsb / macAddress Value为 0X0000000000
Q1.麻烦请分析下原因是代码错误 还是HWREG函数未起作用。
Q2.如何正确debug---》Expressions macAddrLsb / macAddrMsb / macAddress 显示 MAC值
谢谢