This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1310: Sensor controller 的时钟

Part Number: CC1310

大家好:

       请教大家一个问题,CC1310的Sensor Controller 的时钟在我如下的配置下是使用的什么呢?

       1、我用的主晶振为24MHz,外部没有加32.768K的低频晶振,软件配置为休眠模式下使用内部RTC。

       在这种情况下 Sensor Controller 的时钟是怎样的?

      2、遇到的问题,我用Sensor Controller 周期性间隔8s,通过I2C读取一个传感器的数据,目前发现有时会读取失败,在之后就一直不能正常读取,怀疑是I2C时钟问题。