如何使用ADCBuf对多通道的电压值进行连续采样?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
就我我在回调函数里面这里操作会有问题吗?通过init和close来控制adc通道采样,在回调函数中切换采样通道
void adcBufCallback(ADCBuf_Handle handle, ADCBuf_Conversion *conversion, void *completedADCBuffer, uint32_t completedChannel) { /* Adjust raw ADC values and convert them to microvolts */ ADCBuf_adjustRawValues(handle, completedADCBuffer, ADCBUFFERSIZE, completedChannel); ADCBuf_convertAdjustedToMicroVolts(handle, completedChannel, completedADCBuffer, microVoltBuffer, ADCBUFFERSIZE); //数据处理 if(ADCBuf_STATUS_SUCCESS != ADCBuf_convertCancel(adcBuf)) { //while(1); } //采样通道切换 continuousConversion.arg = NULL; continuousConversion.sampleBuffer = sampleBufferOne; continuousConversion.sampleBufferTwo = sampleBufferTwo; continuousConversion.samplesRequestedCount = ADCBUFFERSIZE; switch(step) { case 0: continuousConversion.adcChannel = Board_ADCBUF0CHANNEL2; step = 1; break; case 1: continuousConversion.adcChannel = Board_ADCBUF0CHANNEL3; step = 2; break; case 2: continuousConversion.adcChannel = Board_ADCBUF0CHANNEL4; step = 3; break; case 3: continuousConversion.adcChannel = Board_ADCBUF0CHANNEL5; step = 4; break; case 4: continuousConversion.adcChannel = Board_ADCBUF0CHANNEL6; step = 5; break; case 5: continuousConversion.adcChannel = Board_ADCBUF0CHANNEL7; step = 6; break; case 6: continuousConversion.adcChannel = Board_ADCBUF0CHANNELVDDS; step = 0; break; } /* Start converting. */ if (ADCBuf_convert(adcBuf, &continuousConversion, 1) != ADCBuf_STATUS_SUCCESS) { /* Did not start conversion process correctly. */ while(1); } } bool adc_init() { uint8_t i; if(adcBuf != NULL) { return false; } /* Set up an ADCBuf peripheral in ADCBuf_RECURRENCE_MODE_CONTINUOUS */ ADCBuf_Params_init(&adcBufParams); adcBufParams.callbackFxn = adcBufCallback; adcBufParams.recurrenceMode = ADCBuf_RECURRENCE_MODE_CONTINUOUS; adcBufParams.returnMode = ADCBuf_RETURN_MODE_CALLBACK; adcBufParams.samplingFrequency = 10000; adcBuf = ADCBuf_open(Board_ADCBUF0, &adcBufParams); /* Configure the conversion struct */ continuousConversion.arg = NULL; continuousConversion.adcChannel = Board_ADCBUF0CHANNEL2; continuousConversion.sampleBuffer = sampleBufferOne; continuousConversion.sampleBufferTwo = sampleBufferTwo; continuousConversion.samplesRequestedCount = ADCBUFFERSIZE; if (adcBuf == NULL){ return false; /* ADCBuf failed to open. */ //while(1){} } /* Start converting. */ if (ADCBuf_convert(adcBuf, &continuousConversion, 1) != ADCBuf_STATUS_SUCCESS) { adc_close(); return false; /* Did not start conversion process correctly. */ //while(1){} } return true; } void adc_close() { ADCBufCC26XX_Object *object; if(adcBuf != NULL) { /* Get the pointer to the object and hwAttrs*/ object = adcBuf->object; /* Check if ADC is open and that no other transfer is in progress */ while(!(object->conversionInProgress)); if(ADCBuf_STATUS_SUCCESS != ADCBuf_convertCancel(adcBuf)) { GPIO_write(Board_GPIO_LED1, ON); } ADCBuf_close(adcBuf); adcBuf = NULL; } }