Other Parts Discussed in Thread: CC1200,
TI达人:
如果让CC1120或者CC1200工作在模拟模式下接收数据,能否接收到2-5kbps不同波特率的数据呢?这些数据是否会准确?当然我们可以根据接收到信号的前导码、同步头,如0xAA、0x55之类的脉冲宽度来计算后面数据的波特率。但是我们不清楚CC1120、CC1200芯片能否把正确的抬头信号还原出来。
假设如下:
接收设备:设置CC1120在434.0MHz RX接收模式时,波特率在3kbps,信号输出为模拟模式,输出脚为GPIO3或者GPIO2,通过定时器捕获抬头码计算波特率。
发射设备:设置CC1120在434.0MHz TX接收模式时,波特率在4kbps,2FSK或者是ASK调制格式,发射和接收调制格式是一一对应的。
我的接收设备在波特率在3kbps情况下,能否准确的接收到发送波特率在4kbps的信号吗?