This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1111EMK868-915: CC1111(RFcat)与CC1101通信问题

Part Number: CC1111EMK868-915
Other Parts Discussed in Thread: CC1101

问题描述:

    使用CC1111开发套件(RFcat)与CC1101进行通信时出现解析不了信息。

相关设置:

CC1111作为信号发射,频率915Mhz,比特率384000(实际38360.6),采用OOK调制方式。详细设置如下图所示:

CC1101作为信号接收端,配置为915Mhz,比特率384000(实际38383.5),采用OOK调制方式(附加载波监听),实际配置采用smartRF studio,如下图所示:

使用RFcat(CC1111)发送的时候,载波监听电平有变化,但是在不断跳变,是信号太弱了嘛?

然后使用URH抓信号,发现CC1101和CC1111(RFcat)发送出来的信号载波不太一致,如下图所示:

使用相同频率和采样率抓的信号,CC1101发送波形上图第一个波形所示,发现正弦信号周期为97us。而使用RFcat发送的信号周期为17us,上图第二个波形图。

CC1101之间正常可以传输信号,CC1111传输不了给CC1101。更改CC1111载波频率(从915Mhz切换到315Mhz)发现其载波周期变大,怀疑是RFcat配置问题,想请教一下相关配置,或者说有什么思路?