This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-CC1312R1: 使用LAUNCHXL-CC1312R1开发板debug或者load程序后,开发板无反应,请问怎么使用该开发板?

Part Number: LAUNCHXL-CC1312R1
Other Parts Discussed in Thread: WI-SUN, CC1312R7

新手一枚,买了三块LAUNCHXL-CC1312R1开发板。用开发板包装盒自带的usb连接线连接LAUNCHXL-CC1312R1开发板与电脑(此时开发板绿色指示灯亮着,如图1),并使用Code Composer Studio 11.1.0集成开发环境,选中empty例程(Resource Explorer页面里的Software → SimpleLink SDK → Examples下的例程),点击CCS中的Run下的Debug,红色指示灯闪了几下后一直常量,如图2。或者点击Load,然后红色指示灯闪几下就熄灭了,剩下绿色指示灯常量,和图1一样。接下来就没反映了,empty程序的意思是让LED灯(DIO6的Red的Led灯和DIO7的Green的Led)灯来回切换,频率为1s,但我不论是debug还是load,都自始至终没看见过Led灯闪过。而且按照工程里的Board.html的Jumper Settings说明,我已经拔出了LEDs jumper 和RXD<< and TXD>> jumpers。

请问是什么问题呢?是我哪里操作错误了吗?(注:绿色指示灯、红色指示灯和两个LED没有关系,是不同的灯,在不同的位置)

 图1

 图2