This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-CC1310: 无法同时使用RTC和radio发射

Part Number: LAUNCHXL-CC1310


为了能够精确在每250us发送一次数据,我采用了RTC CH2通道进行定时,然后再主程序中进行radio发送。现在问题是:

1)单独的RTC 程序测试没有问题,通过GPIO电平翻转,可以测试到约250us时刻翻转;

2)单独的射频发送测试没有问题,可通过频谱分析仪测试到发送的信号;

3)将两个合并使用时,则定时器中断可以正常进入;但是射频发送无法进行。

请问,是RTC的使用与RADIO发送冲突了吗?还是使用方法不对导致的?

****************************以下是主程序部分*********************************************************

/*定时器中断处理函数*/
void RTCtimer_int_hanlder(uintptr_t arg)
{
    GPIO_toggle(Board_GPIO_LED0);
    send_flag = 1;
}

/*
 *  ======== adcThread ========
 */
void *adcThread(void *arg0)
{

    ADC_Handle   adc;
    ADC_Params   params;

    /* Call driver init functions */
    RTC_timerCreate(RTCtimer_int_hanlder);
    GPIO_init();
    ADC_init();
    RF_tx_init();
    ADC_Params_init(&params);

    /*配置GPIO*/
    GPIO_setConfig(Board_GPIO_LED0, GPIO_CFG_OUT_STD | GPIO_CFG_OUT_LOW);

    adc = ADC_open(Board_ADC0, &params);
    if (adc == NULL) {
        while (1);
    }

    while(1)
    {
        /*ADC_convert(adc, &adcValue);*/
        if(send_flag == 1)
        {
            send_flag = 0;
            dataNumber++;
            RF_tx_data(adcValue, dataNumber);
        }

    }

****************************定时器程序*********************************************************

typedef struct _RTC_Obj {
    RTC_Fxn                tickFxn;
} RTC_Obj;

static HwiP_Struct RTC_hwiStruct;
static RTC_Obj RTC_handle;


static uint32_t delay_ticks = (uint32_t)(0.00025*FACTOR_SEC_TO_COMP_VAL_FORMAT); /*定时间隔*/


void RTC_init(void)
{

    /*关闭并重置RTC*/
    AONRTCDisable();
    AONRTCReset();

    HWREG(AON_RTC_BASE + AON_RTC_O_SYNC) = 1;
    /* read sync register to complete reset */
    HWREG(AON_RTC_BASE + AON_RTC_O_SYNC);


    /*清除RTC事件*/
    AONRTCEventClear(AON_RTC_CH2);
    IntPendClear(INT_AON_RTC_COMB);

    HWREG(AON_RTC_BASE + AON_RTC_O_SYNC);

}


void RTC_intFxn(uintptr_t arg)
{
    /* clear the RTC event */
    AONRTCEventClear(AON_RTC_CH2);

    RTC_handle.tickFxn(NULL);

}


void RTC_start(void)
{

    uintptr_t key;

    key = HwiP_disable();

    /* reset timer */
    AONRTCReset();
    AONRTCEventClear(AON_RTC_CH2);
    IntPendClear(INT_AON_RTC_COMB);

    /*设置比较值大小*/
    AONRTCModeCh2Set(AON_RTC_MODE_CH2_CONTINUOUS);
    AONRTCCompareValueSet(AON_RTC_CH2, delay_ticks);
    AONRTCIncValueCh2Set(delay_ticks);

    AONEventMcuWakeUpSet(AON_EVENT_MCU_WU0, AON_EVENT_RTC_CH2);
    AONRTCChannelEnable(AON_RTC_CH2);
    AONRTCCombinedEventConfig(AON_RTC_CH2);


    AONRTCEnable();

    /*退出临界区*/
    HwiP_restore(key);
}

void RTC_timerCreate(RTC_Fxn  timer_fxn)
{
    uintptr_t hwiKey;
    /*进入临界区*/
    hwiKey = HwiP_disable();

    HwiP_Params hwiParams;

    HwiP_Params_init(&hwiParams);
    hwiParams.priority = INT_PRI_LEVEL4;
    HwiP_construct(&RTC_hwiStruct, INT_AON_RTC_COMB, RTC_intFxn, &hwiParams);

    RTC_init();
    /*退出临界区*/
    HwiP_restore(hwiKey);

    RTC_handle.tickFxn = timer_fxn;

    RTC_start();
}

****************************射频发送*********************************************************

void RF_tx_init(void)
{

    RF_Params rfParams;
    RF_Params_init(&rfParams);

    if( RFQueue_defineQueue(&dataQueue,
                            txDataEntryBuffer,
                            sizeof(txDataEntryBuffer),
                            NUM_DATA_ENTRIES,
                            MAX_LENGTH + NUM_APPENDED_BYTES))
    {
        /* Failed to allocate space for all data entries */
        while(true);
    }

    RF_cmdTxHS.pQueue = &dataQueue;

    currentDataEntry = (rfc_dataEntryGeneral_t*)&txDataEntryBuffer;
    currentDataEntry->length = PAYLOAD_LENGTH;
    pPacket = &currentDataEntry->data;

    RF_cmdFs_preDef.frequency = 0x0364;   //0x364:868Mhz, 0x0393: 915 MHz
    RF_cmdFs_preDef.fractFreq = 0x0000;

    /* Request access to the radio */
    rfHandle = RF_open(&rfObject, &RF_prop_hsm, (RF_RadioSetup*)&RF_cmdRadioSetup_hsm, &rfParams);


    /* Set the frequency */
    RF_postCmd(rfHandle, (RF_Op*)&RF_cmdFs_preDef, RF_PriorityNormal, NULL, 0);




}

void RF_tx_data(uint16_t playload, uint16_t seqNumber)
{

   /* Create packet with incrementing sequence number and random payload */
    pPacket[0]= (uint8_t)(seqNumber >> 8);
    pPacket[1]= (uint8_t)(seqNumber++);
/*  pPacket[2]= (uint8_t)(playload >> 8);
    pPacket[3]= (uint8_t)(playload);*/

   /* Send packet */
    RF_EventMask terminationReason = RF_postCmd(rfHandle, (RF_Op*)&RF_cmdTxHS,
                                                RF_PriorityNormal, NULL, 0);

}