在USART 0下,我能同时使用UART 用端口P02P03P04P05 ,,SPI 用P12P13P14P15,这样可以同时使用UART,和SPI,传同时使能,有效?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
在USART 0下,我能同时使用UART 用端口P02P03P04P05 ,,SPI 用P12P13P14P15,这样可以同时使用UART,和SPI,传同时使能,有效?
就是说只使用一个USART 0模块,但是要同时作为UART跟SPI?不可行。你可以把USART 0\USART 1分别配置为UART或SPI,这个是可行的。