1. ZigBeeLightLink is not a real time OS, how to add a timer interrupt(100us) ? so that something can be handled in the timer interrupt service routine.
2. how to create an event, like a "periodic send message" function, and add it to the OS?
3. how to copy a scene from one remote to another?
4. where is the location of the list of the connected devices and their status in the flash memory?
5. how to add a function that ends further devices joining to the existing network and how to re-enable it ?
6. if we need to add a new remote to the network, but the old remote lost, how can we join the same network without the old remote?