Description Resource Path Location Type
This project was created using a version of compiler that is not currently installed - 20.2.5.LTS [Arm]. Another version of the compiler will be used during build - 20.2.4.LTS. See 'Help > Install New Software' and select 'Code Generation Tools Updates' to check if this compiler is available through a CCS update. Visit <a href="liveaction:OpenAppCenter">CCS App Center</a> to get the latest compiler support. Or <a href="">software-dl.ti.com/.../a> and install the compiler, then register it with CCS through 'Preferences > CCS > Build > Compilers'. Rx properties Problem