This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1310: CC130 复位时的引脚状态

Part Number: CC1310

HI,

    请问一下,CC1310在上电或是软硬件复位后, 引脚还没初始化之前,引脚是什么状态的呢?

谢谢!

  • Unused I/O Pins By default, the I/O driver (output) and input buffer (input) are disabled (tri-state mode) at power on or reset, and thus the I/O pin can safely be left unconnected (floating). If the I/O pin is in a tri-state condition and connected to a node with a different voltage potential, a small leakage current can go through the pin. The same applies to an I/O pin configured as input, where the pin is connected to a voltage source (for example VDD/2). The input is then an undefined value of either

    0 or 1.