This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1352P: 关于CC1352P1F3芯片的44引脚VDDS和GND之间短路问题

Part Number: CC1352P


你好,我们量产了一批设备,使用的是CC1352P1F3芯片,主要用到射频传输和UART串口通信。在使用中一段时间后出现个别设备的CC1352P芯片不工作的现象,检查发现:万用表测量芯片的烧录口VCC和GND出现短路,然后单独将CC1352P芯片取下来, 测量发现第44引脚VDDS和GND短路。请问:1、出现短路现象可能是什么原因?2、44引脚VDDS是给CC1352P内部的哪些功能模块供电的?

  • 1.短路可能是硬件设计有问题或者是使用过程的外部原因造成短路,建议你对照参考设计检查硬件电路,另外换个使用环境进行交叉测试以确定是不是外部因素影响的

    2.VDDS为整个CC1352P供电

  • 感谢回复,我将对照参考设计检查电路。还有问题是:我这里的5个短路的芯片,都是44号引脚VDDS和GND短路,而13引脚VDDS2和22引脚VDDS3都没有短路,这会是什么原因呢?应该是有区别吧?

  • 对于CC1352P,VDDS_DCDC、VDDS2和VDDS3必须与VDDS处于相同的电位

    在参考设计中,VDDS2和VDDS3与VDDS是连在一起的,短路应该会一起短路

  • 感谢回复。CC1352P 外部电路走线确实是连在一起的,电位也相同。在未将芯片拆下来之前,万用表测量VDDS和GND之间会有几十欧姆到一百多欧姆不等的电阻值(不同损坏设备的电阻值不同),VDDS的电压被拉到2.5V左右(正常3.3V)。但是拆下CC1352P芯片之后单独测量,实际只有芯片的44引脚VDDS短路了(电阻值小于20欧姆),其他VDDS没有短路(电阻值无穷大),这说明在CC1352P内部的每个VDDS引脚是不一样的,有什么不同呢?为什么只有44引脚短路呢?

  • 以下是内部框图,VDDS和VDDS2、3结构不同