This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于CC1110芯片的问题



你好!我是上海移为通信的硬件工程师褚世界,当前我们一个项目使用CC1110芯片,遇到一个问题,特意请教。

就是在调试的时候,发现,如果GPIO口(如P0_0)软件配置成普通的IO输入口时,内部好像有保护二极管存在,这时我们一个外电源通过串联电阻加在此IO口的话,芯片的电源电压VDD会被抬高,使其大于最大工作电压3.6V,从而烧坏芯片,如果配置成ADC输入功能,好像没有漏电,不会影响芯片的VDD。请问,是不是在IO口被配置成ADC功能后,是不是内部的保护二极管,就被禁掉了。

另外,还有一个问题,如果我们的ADC在采样时,输入的模拟电压低于电源电压VDD。但是不需要采样时,会稍高于VDD,大约高了0.4V。请问,这样会有风险吗?

附:我的联系方式:137 6452 1821.   急等回复。谢谢!