This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2531芯片使用问题

Other Parts Discussed in Thread: CC2531, CC2530

本人构想 移植cc2530协议栈到cc2531,组网成功后加上USB转虚拟串口将数据通过USB接口上传给上位机:

目前遇到情况是这样的:协调器建立网络后,路由器加入的时候,我用电源供电有几率进入不了网络,但是我用手乱摸,摸到哪儿不一定突然就能进去发送数据,只要不断电该模块就是正常通信的,一旦掉电,又得乱摸才能进入网络,焊接应该是没问题的,我在调试的时候发现卡在MAC_RADIO_TIMER_WAKE_UP();这个函数了。

我只用了一个32M晶振,协议栈的HAL_BOARD_INIT()

SLEEPCMD &= ~OSC_PD;                       /* turn on 16MHz RC and 32MHz XOSC */                \
  while (!(SLEEPSTA & XOSC_STB));            /* wait for 32MHz XOSC stable */                     \
  asm("NOP");                                /* chip bug workaround */                            \
  for (i=0; i<504; i++) asm("NOP");          /* Require 63us delay for all revs */                \
  CLKCONCMD = (CLKCONCMD_32MHZ | OSC_32KHZ); /* Select 32MHz XOSC and the source for 32K clock */ \
  while (CLKCONSTA != (CLKCONCMD_32MHZ | OSC_32KHZ)); /* Wait for the change to be effective */   \
  SLEEPCMD |= OSC_PD;                        /* turn off 16MHz RC */                              \
                                                                 \
  /* Turn on cache prefetch mode */                              \
  PREFETCH_ENABLE();                                             \
                                                                 \
  HAL_TURN_OFF_LED1();                                           \
  LED1_DDR |= LED1_BV;                                           \
  HAL_TURN_OFF_LED2();                                           \
  LED2_DDR |= LED2_BV;  

这种现象是什么造成的,是静电吗,还是硬件哪里地没接通,还是说我再哪里配置出问题了呢,目前的HAL_UART_USB我设置为0,因为USB部分现在还没有做

NV-RESTORE我在编译预选项中是加入了的