CC1310 (RHB)5x5封装的芯片的DIO_7,在未初始化IO口模式的时候,是保持什么状态?
如果未配置的引脚连接到具有不同电压点位的节点,是否会有漏电流产生?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Unused I/O Pins By default, the I/O driver (output) and input buffer (input) are disabled (tri-state mode) at power on or reset, and thus the I/O pin can safely be left unconnected (floating). If the I/O pin is in a tri-state condition and connected to a node with a different voltage potential, a small leakage current can go through the pin. The same applies to an I/O pin configured as input, where the pin is connected to a voltage source (for example VDD/2). The input is then an undefined value of either 0 or 1.