TI的技术支持工程师您好!目前,我正在使用贵公司的CC2541,开发产品,但是遇到问题需要请教。在设计中,利用SPI模块与其他模块通信,接收数据成功后触发DMA读取数据,DMA将数据读取完毕后产生DMA中断,通知CPU。。。。。另外,在程序中利用Timer3设计了一个时基定时,定时时间为8ms。。。。现在的问题是,由于DMA读取SPI数据并产生中断需要连续多次进行,所以导致一段时间内(大概30ms,DMA中断的运行时间和每两次间隔,经测试都是12us),Timer3无法进入中断了,从而导致时基不准确。
现在我想知道,在设计CC2541时,有没有在DMA中断前后的一段时间内,其他中断是无法触发的例子呢?或者可否提供CC2541芯片的DMA更详细的应用手册呢?