各位大侠您好:
小菜想尝试使用TI的蓝牙4.0芯片cc2540做蓝牙遥控器,电源使用型号为:cr2450的纽扣电池,遥控器做出来,也能正常使用,就是使用寿命太短,大概是一天左右,以下是纽扣电池的基本参数:
容量:600mAh
持续工作电流:0.2mA;
恒定输出电压:3V
有没更好的方案可以延长电池的寿命大概到一年(每天平均持续使用2小时),或者有没有更好的纽扣电池适合做蓝牙遥控器的电源??请各位大侠指点,谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.