hi 各位:
现在我使用的芯片是cc2540,代码是主机代码, 测试了一下消耗电压。
PM3睡眠模式:13h消耗电压是2.90V-2.90V=0V
Low MCU activity: 32-MHz XOSC running 正常模式:2h消耗电压是2.90V-2.62V=0.28V
TX or RX mode:30m消耗电压是2.62V-2.43V=0.19V
请教一下如何让正常模式和TX or RX mode有更低的功耗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.