This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1310: 2-3米范围内的最高传输速率

Part Number: CC1310

请问有人实现过cc1310在2-3米范围内的最高传输速率吗?

本人需要在2-3米内实现2Mbps以上稳定无线传输,蓝牙达不到要求,WIFI功耗太高,看cc1310的手册可以实现4M传输,也有论坛里的小伙伴说4M下误码率17%非常高(但不清楚距离)

cc1310是可以实现公里级别传输的,在2-3米范围内误码率是否会降得很低?

  • 高速率下误码率是会有所上升,没测过4Mbps下2-3米的误码率,距离较近的情况下PER大概在5%左右

    你可以使用例程C:\ti\simplelink_cc13x0_sdk_4_20_01_03\examples\rtos\CC1310_LAUNCHXL\drivers\rfPacketErrorRate来测试