This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1310: IO口引脚配置

Part Number: CC1310

我在CC1310的SDK中看到,芯片可操作性的io口共有32个,为DIO0-DIO31;但是不同封装的芯片,引出的io引脚不足32个;

以RHB封装的CC1310芯片为例,引出的IO口为DIO0-DIO14;

问题1:未引出的DIO15-DIO31是否还能配置引脚模式?

问题2:在不配置DIO15-DIO31的引脚模式的情况下,是不是就会保持3态?