我在使用CC1352P的时遇到了一个问题,在采用SUB1G模式(设置为:200kbps,50kHz Deviation,2-GFSK,311kHz RX Bandwith),高功率口采用巴伦,低功率口是单端外偏接收,在采用射频线缆连接时,接收灵敏度小于-95dBm,但是用天线发射接收,灵敏度就在-70~-80dBm之间,放在屏蔽箱中测试也是如此。2.4G测试都是正常的。下面是原理图:
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我在使用CC1352P的时遇到了一个问题,在采用SUB1G模式(设置为:200kbps,50kHz Deviation,2-GFSK,311kHz RX Bandwith),高功率口采用巴伦,低功率口是单端外偏接收,在采用射频线缆连接时,接收灵敏度小于-95dBm,但是用天线发射接收,灵敏度就在-70~-80dBm之间,放在屏蔽箱中测试也是如此。2.4G测试都是正常的。下面是原理图:
在采用射频线缆连接时,接收灵敏度小于-95dBm,但是用天线发射接收,灵敏度就在-70~-80dBm之间
是在发射功率多大的技术上测试的,传导测试-95dB看起来是正常的,辐射测试的结果与天线辐射效率有关
阻抗不匹配、天线尺寸、测试方向都会影响测试结果
发射都是用20dBm高功率口,射频线缆连接,灵敏度是正常的,同样的天线装在TI的Demo板上是正常的,不同方向都已经测试过了,效果一样,最大差别就是差分接收和单端接收,单端接收时,会不会是板子上接收到的空间辐射耦合进去导致数据校验错误呢?测试时,接收到的RSSI值跟Demo板做过对比,比Demo小2-3dBm,这个正常,只是收到数据错了很多,无法正确解析。
我想不到其他原因了
在英文论坛看到你也发了帖子,按这里的步骤提交硬件审查,以确定硬件是否有问题:https://www.ti.com/tool/SIMPLELINK-SUB1GHZ-DESIGN-REVIEWS