在远距离通讯应用中,最优条件下CC1352P7的通讯距离和LORA(sx1268)比怎么样?从数据上看CC1352P7的接收灵敏度-121dBm(在 2.5kbps 远距离模式下),sx1268接收灵敏度-148dBm似乎要强一些。CC1352P7采用鞭状天线在野外一般通讯距离多远?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
在远距离通讯应用中,最优条件下CC1352P7的通讯距离和LORA(sx1268)比怎么样?从数据上看CC1352P7的接收灵敏度-121dBm(在 2.5kbps 远距离模式下),sx1268接收灵敏度-148dBm似乎要强一些。CC1352P7采用鞭状天线在野外一般通讯距离多远?
CC1352P7的发射功率最大10dB,sx1268的发射功率最大22dB.
CC1352P7最大发射功率是20dBm,在433M由于SRRC法规的限制,只能使用10dBm
可达到的最大距离与频率、发射功率、接收灵敏度、数据速率以及环境噪声都有关,另外要达到最大距离需要使用外部天线
我们之前在挪威环境噪声小的户外测试的CC13xx系列最大点对点通信距离可达到20公里左右