This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1310: CC1310 开机瞬态电流

Part Number: CC1310


在CC1310 规格书  5.4 Power Consumption Summary  有描述相关电流

此项目使用电力场合,使用了特殊AC/DC 器件 ,其中元件规格书上有描述

input voltage again rises above the UVLO rising threshold.
During this time the output voltage will be loaded by less
than 100nA. 

在特殊供电后 AC/DC 元件输出电压 DC  3.6V  静态电流 89nA ,

供电时间250秒后 VOUT  3.6V ,电流可达到50mA 。

问题. CC1310 开机瞬态电流最低需要多少 ,其中 无功能的  IO 是否需要接地。

在 250秒之内,CC1310 VDDR 已经改为 1.65V输出。是否还需要其他改动