This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1310: 发射时电流问题

Part Number: CC1310
Other Parts Discussed in Thread: CC1101, CC2500

// Parameter summary
// RX Address0: 0xAA
// RX Address1: 0xBB
// RX Address Mode: No address check
// Frequency: 433.92032 MHz
// Data Format: Serial mode disable
// Deviation: 5.000 kHz
// Packet Length Config: Variable
// Max Packet Length: 255
// Packet Length: 20
// Packet Data: 255
// RX Filter BW: 49 kHz
// Symbol Rate: 17.99927 kBaud
// Sync Word Length: 32 Bits
// TX Power: 15 dBm (requires define CCFG_FORCE_VDDR_HH = 1 in ccfg.c, see CC13xx/CC26xx Technical Reference Manual)
// Whitening: CC1101/CC2500 compatible

使用以上设置,之前一直都是pcba测试,发射时最大电流(指针毫安电流表)到8~10mA。后面把pcba装到硅胶材质外壳中,实测发射电流变大会到20mA。这是之前发的帖子。

后面只修改发射功率值,其他不变,测得下表。(使用RF studio测试)

5KBPS SLR mA mA
序号 TX POWER pcba电流 距离 RSSI 硅胶电流 距离 RSSI
1 15 10 -49 15 -43.7
2 13.7 9 -49 14 -43.4
3 12 9 -54 10.5 -49
4 10 8~9 -52.2 9 -47
5 8 8 -53 8 -53
6 6 7 -60 7 -60
7 4
8 2 7 -69 7 -69
9 0
10 -10

改小发射功率后,可以看见RSSI是明显小了,但是单次发射电流不会明显减小,显示7mA左右。

问题:

1 改变发射功率值后芯片内部是如何调整发射功率?修改发射电压?

2 修改发射功率并不能明显减小发射电流,那想减小单次发射电流是不是只能选择高的传输速率,缩短发射时间了?

  • 您好,

    收到您的问题了,我们升级到英文论坛给工程师看下,有答复尽快给到您。

  • 1.修改CCFG  #define CCFG_FORCE_VDDR_HH 0x0 // Use default VDDR trim                              //低功率模式  VDDR 1.65V
                         // #define CCFG_FORCE_VDDR_HH 0x1 // Force VDDR voltage to the factory HH setting (FCFG1..VDDR_TRIM_HH)   //高功率模式 vddr 1.95V

    2. 功率 在10dbm  电流消耗 约 13.2mA   15dbm    25mA 具体可查看规格书 & 功率影响距离

    建议 RF 在整机情况下做RF匹配 电路,具体与天线厂合作调试电路 ,没有做匹配的测试不准确