This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

蓝牙连接断掉问题

Other Parts Discussed in Thread: CC2540

Hi 各位:

        我在使用cc2540做的蓝牙遥控器(主机)连接从机时,出现了一个这样的现象:分别设置连接间隔最大值和最小值都为32,即:

        GAP_SetParamValue(TGAP_CONN_EST_INT_MIN,32);
        GAP_SetParamValue(TGAP_CONN_EST_INT_MAX,32); 这种情况下连接上后不容易断掉,

       当我:分别设置连接间隔最大值和最小值都为80,即:       

        GAP_SetParamValue(TGAP_CONN_EST_INT_MIN,80);

        GAP_SetParamValue(TGAP_CONN_EST_INT_MAX,80); 连接上后很容易就出现连接断掉,断掉的原因是:0X3E,请各位知道,为什么使用 

      参数为80会怎么容易出错,如果我保持设置参数为80,能有方法使连接上后不会立即断掉吗?谢谢各位