在tirtos_cc13xx_cc26xx_setupwin32_2_21_01_08版本的SDK中,我在例程的CC1310_LAUNCHXL.c中看到如下注释:
/*
* ========================= IO driver initialization =========================
* From main, PIN_init(BoardGpioInitTable) should be called to setup safe
* settings for this board.
* When a pin is allocated and then de-allocated, it will revert to the state
* configured in this table.
*/
我有以下疑问:
首先,在在uartCC26XXHWAttrs结构体中将DIO4设置为串口的TX脚。
随后,在BoardGpioInitTable中将DIO4设置为输入上拉模式,并且在main函数中,执行了PIN_init(BoardGpioInitTable)动作。
然后开启串口并发送数据。数据发送完成后将串口关闭,此时DIO4是不是会自动恢复到上拉输入模式?