This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我如果把POWER_SAVING宏去掉,就能够一直advertise
我现在跟踪调试,发现demo中的PM2模式似乎唤不醒芯片,在halSleepTimerIsr中设断点没有拦截到
在CC2541的文档中看到:
The Sleep Timer is also used to maintain timing in Timer 2 when entering power mode
PM1 or PM2.
When Timer 2 is used together
with the Sleep Timer, the timing function is provided even when the system enters low-power modes PM1
and PM2.
跟Timer2一起用会影响到Sleep Timer的唤醒功能吗