本人采用CC3235S-LAUNCHPAD上的XDS110连接了自己电路板上的CC1310进行debug和使用SmartRF软件进行在线通信都不成功
首先自己设计的电路板上的CC1310连接到CC1310-LAUNCHPAD上的XDS110时,一切功能都是正常的,比如进入Debug模式和使用SmartRF软件进行通信测试都是成功的,
但是将相同的CC1310连接到CC3235S-LAUNCHPAD上后则会出现问题。
问题描述如下:
CC1310通过JTAG与CC3235S-LAUNCHPAD上的XDS110连接,连接实物图如下:

在这种连接情况下,利用CCS测试JTAG连接情况,结果显示连接正常
但是在进入Debug模式时,报错:Error -260
Error initializing emulator:
(Error -260 @ 0x0)
An attempt to connect to the XDS110 failed.The cause may be one or more of: no XDS110 is connected, invalid firmware update, invalid XDS110 serial number, or faulty USB cable. The firmware and serial number may be updated using the xdsdfu utility found in the .../ccs_base/common/uscif/xds110 directory of your installation. View the XDS110SupportReadMe.pdf
file there for instructions.
并且在利用SmartRF软件进行在线射频通信测试时,无法打开在线通信界面,报错

我想请问一下,为什么使用CC3235S-LAUNCHPAD上的XDS110就会遇到问题,但使用CC1310-LAUNCHPAD上的XDS110则没有问题呢,这个问题又是因为什么产生的呢?