This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

蓝牙BLE版本 如何支持一点到多点通讯?



正在研究蓝牙的相关信息,请问谁知道BLE版本如何支持点到多点?以前的版本是先通过Piconet 支持1主7从,然后Scatternet进行网络拓扑。我看蓝牙的网站上对BLE网络拓扑那里只提到了Topology – Bluetooth low energy technology uses a 32 bit access address on every packet for each slave, allowing billions of devices to be connected. The technology is optimized for one-to-one connections while allowing one-to-many connections using a star topology. With the use of quick connections and disconnections, data can move in a mesh-like topology without the complexities of maintaining a mesh network.  是否意味着现在是直接可以进行一点到无限个多点的通讯?每个BLE芯片都支持这一技术么?