This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2541 ADC转换

Other Parts Discussed in Thread: CC2541

请教一下:

 我的板子使用锂电池,然后通过一个3V输出的LDO来给CC2541芯片供电。然后我用1:1的两个电阻来给VBAT分压,中间接的是AIN7,也就是我要用AIN7来测量电压,进而获取VBAT的值。

但是我发现单步执行的时候测量的值是对的,但是正常的运行时候值就偏大了。

是不是ADC转换时间 不够?

  • What is the resistor value in "1:1的两个电阻来给VBAT分压" ?

    The input resistance of ADC is typical 197kOhm in datasheet.

    Generally, a much lower resisitor should be use for the potential divider for VBAT. A transistor may needed for switch on the divider part for ADC measurement and switch off when no ADC measuremnet to save power.