TI工程师:
您好! 我在开发产品中,发现芯片设置为WOR模块,发现设置的WOR醒来时间是不定的。比如我设置的是5mS,但是实际过程中可能会出现WOR醒来的时间有时会变成15mS。 因为设置的是低功耗产品,对功耗有要求。 希望能得到你们的帮助!谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好。
我好奇既然你要低功耗为什么还只休眠5mS ?根据文档说明WOR好像是至少200uA吧,根本用不到多长时间。
定时不准我也遇到过,不过我们要求很低,几分钟误差都没问题,我出现几秒就也没在意了。
我不知道你如何测量周期时间,你怎么记录开始睡眠时间和唤醒时间?我意思是如果中间还有其他事情在做的时候会不会因为这样产生延时了(你只是假定你运行代码均时)?
Chao,
您好!
您使用的是CC1100E么? 如果是的话,请参考数据手册51页右下方的描述:
If any frequency programming register is
altered when the frequency synthesizer is
running, the synthesizer may give an
undesired response. Hence, the frequency
programming should only be updated when
the radio is in the IDLE state.
所以请在IDLE模式下配置这些参数。谢谢!