手上项目要做433M的无线设备,看到TI两个系列的433M片上系统,CC1110和CC43,还了解到那个无线电唤醒功能(wake-on-radio)
请问,
1. wake-on-radio(wor)这个功能有没有相关的资料和例程的?
2. CC1110系列是否具有wake-on-radio功能?
3. CC430系列是否全系列具有这个功能呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello wei,
1. Wake-On-Radio(WOR)是收发器的一个功能,可以使收发器在没有MCU干预的情况下,周期性地醒来听一下看看有没有数据包。
具体可参考AN047:http://www.ti.com/lit/an/swra126b/swra126b.pdf
2. CC1110和CC430系列均属于SoC,它们的MCU需要醒来才能使其radio进入Rx模式,因此wake-on-radio(wor)的概念并不适用于它们。
3. 对于SoC芯片,可以直接设置其为polling receiver,具体请参考DN111:http://www.ti.com/lit/an/swra207a/swra207a.pdf
Best regards
Martin Li