最近用TIVA C调试CC1101,怎么也调不通,发送部分应该没问题,接收部分好像有问题,,,,有几个问题需要向各位大神请教一下~~~
1,例程好多都是CC1100的,能和1101的通用么?
2,将发送部分模块的GDO0设置为0X06,即Asserts when sync word has been sent / received, and de-asserts at the end of the packet.
发送之前,读取了TXBYTES寄存器,为0,写了TXFIFO以后,读取TXBYTES为理想的数据.发送命令STX以后,检测到GDO0的低-高-低跳变,而且TXBYTES为0,是否意味着发送部分没问题了呢??
3.接收部分,在IDLE模式下,给发命令,SRX,使之进入接收模式,为什么有时候会进去,有时候进不去呢?
4,接受部分和发送部分采用完全相同的配置,为什么接收部分总是收不到信息呢?RXBYTES总是为0,有时候竟然是乱码,随机数;.
不胜感谢~