This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Z-stack OTA Upgrade user's guide



我用的是smartRF05 with CC2530ZDK_EM。手册中12页

3)

Build the Project.

a.Verify the active project in the Workspace toolbar is Debug

toolbar里没有Debug选项。

12页最后一行,b.Verify the In EndDeviceEB-Pro configuration is selected没有EndDeviceEB-Pro 选项。

15页3)b.Verify the In Premise Display – OTA configuration is selected中没有Premise Display – OTA 选项。

怎么解决这些问题。谢谢!

版本号是:ZStack-CC2530-2.4.0-1.4.0

  • 这篇文档是针对  Sample OTA Application 来写的,请注意3.2 章节! This section describes the process of building and downloading the Sample OTA Application. Two boards need to be programmed. One board will run the OTA Dongle application and is called the Dongle. One  该样例程序在x:\Texas Instruments\ZStack-CC2530-2.4.0-1.4.0\Projects\zstack\HomeAutomation\SampleSwitchOta