This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

无线智能仪表控制



各位老师,我现在想做这样一个系统:安装一个水表,将水流数据实时的无线传送到2公里外的控制中心。控制中心可以根据这个数据,发送无线控制信号反馈回去控制阀门从而控制水流,以保证水流大小在控制范围内。请问可以采用哪些器件做成这个方案? 谢谢了。

  • 。。。。。。又是毕业设计?首先你要搞清楚

    (1)水流的流量传感器要用哪种?

    (2)控制阀门用哪种?步进电机控制的?还是小流量的用电磁阀PWM通断来控制?

    (3)2公里,如果数据量不大,最好用400MHz的RF模块吧,数据量大就要用900Mhz或2.4G的,或用个GPRS模块吧,无距离限制,有信号就行了

    (4)控制中心指的是什么?电脑自动控制?人工控制?电脑控制的话就要考虑UART接口或USB接口或LAN接口,人工控制的话。。。。。无要求

    这些都没搞清楚就来讨方案是没人理的,这里可以做技术讨论区,不是老师授课区