求解,在使用time3 PWM输出时,编译器debug时一直提示idata溢出
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
寄存器配置应该不会有问题,代码如下:
/* Setup TIMER3 PWM at alternate location 2 */
PERCFG |= 0x20; // TIME3 at location 2
P1SEL |= 0x40; // Peripheral function on TIMER3 (P1_6 P1_7)
P2SEL |= 0x20; // Give priority to TIMER3 over USART 1 for P1_6 P1_7 pins.
//set the time ticks to 32M , CLKCONCMD[5:3]
CLKCONCMD &= ~0x08;
CLKCONCMD &= ~0x10;
CLKCONCMD &= ~0x20;
//set the Prescaler divider to 128
T3CTL |= 0x80;
T3CTL |= 0x40;
T3CTL |= 0x20;
//set the timer3 mode
T3CTL |= 0x03; //up/down
//set the time3 channel0 mode
T3CCTL0 |= 0x04; //compare mode
T3CCTL0 |= 0x20; //clear output on compare_up,set on 0
T3CCTL0 &= ~0x10;
T3CCTL0 &= ~0x08;
//clear counter
T3CTL |= 0x04;
//set the compare value
T3CC0 = 0x40;
//set the interrupt
T3CTL |= 0x08; //overflow interrupt mask
T3CCTL0 |= 0x40; //channel 0 interrupt mask
IEN0 |= 0x80; //enable interrupt
IEN1 |= 0x08; //timer3 interrupt enable
// //start the pwm
T3CTL |= 0x10;
还有如果我在上面的代码后面加while(1)pwm波形输出正常,但是去掉while(1)后,系统跑起来后看波形根本没按设定的速率输出,一点规律没有